This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6455 Linker Errors

I'm porting a project from MSVS 2008 to the C6455. The code executes as expected on a PC.

The CCS linker has the following unresolved symbols as shown below.

Code Gen Tools: 6.1.11

DSP/BIOS: 5.33.05

RTS Lib: rts64plus_eh.lib - this file is last in the link order

undefined symbol:   std::_Facetptr<T1>::_Psave [with T1=std::num_put<char, std::ostreambuf_iterator<char, std::char_traits<char>>>] 
first referenced in file: C:\\JvmfParserPackage\\JVMF_Parser_CCS_v1\\SWB1\\upc_board\\SWB1.lib<astsParserSWB1.obj>

undefined symbol: std::_Facetptr<T1>::_Psave [with T1=std::ctype<char>]
first referenced in file: C:\\JvmfParserPackage\\JVMF_Parser_CCS_v1\\SWB1\\upc_board\\SWB1.lib<astsParserSWB1.obj>

undefined symbol: std::_Facetptr<T1>::_Psave [with T1=std::numpunct<char>]
first referenced in file: C:\\JvmfParserPackage\\JVMF_Parser_CCS_v1\\SWB1\\upc_board\\SWB1.lib<astsParserSWB1.obj>

undefined symbol: std::fpos<T1>::_Stz [with T1=int]
first referenced in file: C:\\JvmfParserPackage\\JVMF_Parser_CCS_v1\\SWB1\\upc_board\\SWB1.lib<astsParserSWB1.obj>

undefined symbol: std::numpunct<T1>::id [with T1=char]
first referenced in file: C:\\JvmfParserPackage\\JVMF_Parser_CCS_v1\\SWB1\\upc_board\\SWB1.lib<astsParserSWB1.obj>

undefined symbol: std::num_put<T1, T2>::id [with T1=char, T2=std::ostreambuf_iterator<char, std::char_traits<char>>]
first referenced in file: C:\\JvmfParserPackage\\JVMF_Parser_CCS_v1\\SWB1\\upc_board\\SWB1.lib<astsParserSWB1.obj>

undefined symbol: std::basic_string<T1, T2, T3>::npos [with T1=char, T2=std::char_traits<char>, T3=std::allocator<char>]
first referenced in file: C:\\JvmfParserPackage\\JVMF_Parser_CCS_v1\\PM\\upc_board\\PM.lib<ParserManager.obj>