This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3703 VFP Clock Cycles

Does it really take on the order of 18-21 clock cycles to perform one single precision floating point operation via the VFP (VFPv3 lite)?

I was under the assumption that it was more like 1-2 clock cycles.  Apparently there are a number of versions of the VFP (according to the ARM site), some of which can do over 1 FLOP per clock cycle, but not the one in the 3703?

Can you confirm the number of clock cycles for the VFP when performing a single precision floating point operation via the VFP on the AM37073 please.