Other Parts Discussed in Thread: AM3354
All,
I have 2 focus customers looking to substitute AM3354/6/8's for the AM3352 for part availability.
While it looks easy (if matching temperature and package), the devil is in the details.
I assume there is a product ID that might have to be added to the firmware if their firmware team has accessed it.
One customer brought up speed grades and noted that Linux would try and run at the fastest speeds so if a 3358 1GHz part was substituted Linux would run faster than their thermal envelope at 800MHz on the 3352.
This doesn't sound right to me - but the datasheet was ambiguous.
Thoughts on pitfalls to watch for?
Thanks!
Blake