Recently, I update my CCS3.3 with the SP12 and CGT (6.1.5) for my C6455 development. However, I just found out that using this update CCS is generating different .out file, which will output incorrect results.
Previously, I used the CCS3.3 without these update, and the running results were the same as I expected. However, when I use the updated CCS3.3, the running results were with big error. So I thought it is maybe the different setting of the building option, especially for the compiler. So, I distable all the optimization and re-compile my code. I run the program and there is an error displayed in the stdout window as following:
The CIO command cmd:(0) in the CIO buffer at address (0x9e8d80) was not recognized. Please check the device and program memory maps.
Then, I only got a portion of all the outputs. However, based on these incomplete outputs, I can see these results are correct. This really makes me feel that the previous inconsistent results is due to the setting for the build option.
So, Can any one give me some hints: (1)what is the reason for above error in the stdout window (2)what should I do to make this update CCS generate the same results as I got using the original CCS (without these updates)
Thank you so much,
Renaissance.