Other Parts Discussed in Thread: SYSCONFIG
Hi team,
Here's an issue from the customer may need your help:
PDK Version 08_04
1) Failed to configure interrupt routing:
Call to Sciclient_rmIrqSet failed to return, traced and discovered it was caused by a return error from [Sciclient_rmIrqFindRoute].
The configuration code is as follows:
struct tisci_msg_rm_irq_set_req rmIrqReq;
struct tisci_msg_rm_irq_set_resp rmIrqResp;
uint32 retVal;
rmIrqReq.valid_params = TISCI_MSG_VALUE_RM_DST_ID_VALID;
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID;
rmIrqReq.src_id = TISCI_DEV_MCSPI0;
rmIrqReq.global_event = 0U;
rmIrqReq.src_index = 0U;
rmIrqReq.dst_id = TISCI_DEV_MCU_R5FSS0_CORE0;
rmIrqReq.dst_host_irq = CSLR_MCU_R5FSS0_CORE0_INTR_MAIN2MCU_LVL_INTRTR0_OUTL_0 + 1;
rmIrqReq.ia_id = 0U;
rmIrqReq.vint = 0U;
rmIrqReq.vint_status_bit_index = 0U;
rmIrqReq.secondary_host = TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST;
retVal = Sciclient_rmIrqSet(&rmIrqReq, &rmIrqResp, SCICLIENT_SERVICE_WAIT_FOREVER);
if((uint32)0 != retVal)
{
ERR("Sciclient_rmIrqSet[%s] interrupt cfg err!", g_name_list[chn]);
}
2) MCSPI0 initialization failed:
Call to MCAL [SPI_Init] is stuck, traced and found after execute to [SPI_mcspiReset], program is stuck while writing [sysconfig] register and no return.
SPI_FUNC_TEXT_SECTION static void Spi_mcspiReset(uint32 baseAddr)
{
StatusType status;
TickType startCount = 0U, tempCount, elaspsedCount = 0U;
/* Set the SOFTRESET field of MCSPI_SYSCONFIG register. */
CSL_REG32_FINS(
baseAddr + MCSPI_SYSCONFIG,
MCSPI_SYSCONFIG_SOFTRESET,
MCSPI_SYSCONFIG_SOFTRESET_ON);
....
}
Could you help check this case? Thanks.
Best Regards,
Cherry