Part Number: TDA4VM
Hi team,
Here's an issue from the customer may need your help:
Using the ti-processor-SDK-RTOS-j721e-EVM-08_04_00_06 original code.
The customer wants to add a DIO driver to the code of MCU2-0 to drive the LED8 and LED9 user lights on the EVM board to drive the can to send messages out. But they don't know how to add these drivers to the project to build.
Is it required to copy the contents of MCUSW or just need to call MCAL directly?
Also, is it important that MCAL code be configured with the EB tool? Is there a drive for a non-EB tool available?
Could you help check this case? Thanks.
Best Regards,
Cherry