Part Number: SK-TDA4VM
Other Parts Discussed in Thread: TDA4VM
1.HI,We tested the performance of qbu, such as message latency。
2.We compare the delay of receiving and sending high priority messages,when the qbu is enabled and not enabled.
3.We found that,after the qbu is enabled, the delay is not greatly improved.
4.We send data through iperf, and at the same time we send data through sockets in user space,like this:
iperf3 -c 192.168.100.20 -u -b500M -l1472 -t300
iperf3 -s
It mapped to queue 0.
5.And ethtool -l eth0 like this:

6.Then we send data through sockets in user space with priority 3,result like this:

gap1 is the delay of receiving and sending high priority messages.
7.Without qbu,the result is like this:

8.After the qbu is enabled, the delay is not greatly improved.
Can you tell me why is this result?