I have a LogicPD AM3517 Experimenter board.
This comes with a minimal Linux installation.
It was suggested that I create an SD Card boot of the latest Linux SDK for Sitara which I did.
The version is at
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/sdk/AM3517/latest/index_FDS.html
and is the ti-sdk-am3517-evm-04.01.00.00-Linux-x86-Install
The SD Card boot appears to be working but then hangs just after the message
"Calibrating touchscreen (first time only)"
The EVM has a touchscreen on the app board but the Experimenter has no touchscreen and this should not hang.
If needed I could send the terminal output during the boot phase.
Any advice on making a code change to fix this so I can proceed?