Part Number: TMS320C6657
Hello expert,
Regarding the TMS320C6657 family , I want to konw whether TMS320C6657CZHA25 can be replace by TMS320C6657CZH25 ?
If I use only 1.1Ghz, whether the 1.25Ghz can cover ? Any pin can set the freqency ?
Many thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6657
Hello expert,
Regarding the TMS320C6657 family , I want to konw whether TMS320C6657CZHA25 can be replace by TMS320C6657CZH25 ?
If I use only 1.1Ghz, whether the 1.25Ghz can cover ? Any pin can set the freqency ?
Many thanks!
Dear Customer,
Regarding the TMS320C6657 family , I want to konw whether TMS320C6657CZHA25 can be replace by TMS320C6657CZH25 ?
If I use only 1.1Ghz, whether the 1.25Ghz can cover ? Any pin can set the freqency ?
Answer for Q1:
=============
In the part number, "TMS320C6657CZHA25 ", Here the "A" stands for TEMPERATURE RANGE
A = Extended temperature range (-40°C to +100°C)
S = Extended low temperature range (-55°C to +100°C)
---
In the part number, "TMS320C6657CZH25 ", Here the "Blank" means
Blank = 0°C to +85°C (default case temperature)
--
Answer for Q2:
==============
The max core frequency that the processor-device-run is at 1.25 GHz. We can run at frequencies at 600MHz, 800MHz, 1000MHz (i.e., 1 GHz) etc....
Visit the https://www.ti.com/lit/ds/symlink/tms320c6657.pdf datasheet for more info.
Regards
Shankari G