Customer is using version E3 of SK-AM62.
They want to connect a display panel to J21 connector of SK-AM62. Is there a recommended panel and part number?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Eddie Koh
Thank you for the query.
I am checking internally and will update you.
Regards,
Sreenivasa
Hello Eddie Koh,
Please refer below
Microtips panels (interfaced to AM62 SK and AM62Q SK):
13-101HIEBCAF0 -> w/ touch support
13-101HIEB0HF0 -> w/o touch support
Regards,
Sreenivasa
Hello Eddie Koh,
I added additional inputs that i received.
For the Microtips panel the SW team already published the code[1].
Regards,
Sreenivasa
Sreenivasa,
Seems the LVDS connector signals definition is not compatible with that of 13-101HIEBCAF0, is there a adaptor board?
The connector on SK E3 is:
on 13-101HIEBCAF0 is
Hello Tony,
Thank you for checking.
The display expert is on vacation this week.
Let me check and update.
Regards,
Sreenivasa
Yes, we have an adapter board on the LCD. Please refer to the attached LCD adapter board MF-101HIEBCAF0-C_DSN.pdfschematics.