Hello Champs,
Customer failed to add Cdd_IPC module, EB prompted below error. 
Thanks
Rgds
Shine
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Which version of SDK/Config are you using? For example:
SDK 8.2, MCUSW_01_03_04_01_CONFIG-windows-installer.exe.
Regards,
Erick
Hi Erick,
Thanks for your help.
Customer uses SDK 8.4 pdk_j7200_08_04_00_19 on linux.
Thanks.
Rgds
Shine
Hello Shine,
I've taken the configuration that comes along with this SDK version (MCUSW_01_05_00_01_CONFIG), created a fresh copy of it into the plugins folder of the EB Tresos installation and generated the code with no issues.
Firstly, has the customer modified the configuration at all, or is it the default configuration?
One thing to note, if you update the configuration Plugins in the EB/tresos/plugins folder, you will need to make sure that Tresos is not currently running, and once you have copied over the new configurations, you can open it again.
Regards,
Erick