This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI 1271 wifi driver and ipv6

Dear Sirs:

  We are using 1271 wifi module at a zoran 4310 platfrom, which has two interfaces (eth0 and wlan0). IPv6 works fine via eth0. But it doesn't work for wlan0.  We can't ping to another device by its ipv6 link local address. We aslo fail to ping this 1271 link local address at another device. Ipv4 is ok. Is there anybody know whether ipv6 is supported by 1271 wifi driver or what I should setup? Thanks.

PS: My Access point is DLink Dir-615, which support ipv6.

wlan0     Link encap:Ethernet  HWaddr 08:00:28:AB:CD:99
          inet addr:192.168.0.102  Bcast:192.168.0.255  Mask:255.255.255.0
          inet6 addr: fe80::a00:28ff:feab:cd99/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:19 errors:0 dropped:0 overruns:0 frame:0
          TX packets:14 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:100
          RX bytes:6282 (6.1 KiB)  TX bytes:3598 (3.5 KiB)

Best Regards.

Wenson 2011/6/13