This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About DM365DVR source code



Hello everyone,

We bought a DM365DVR board some months ago.  And we need to custom the web view now, but we can't find the EVSWebCtrl source code in the RDK.

Coulde anybody tell me how I can custom the web view?

 

Thanks

Yanbin Yue

  • Hi,

    The source code of the web view is not available as part of RDK. By default, it comes as binary in RDK release package.

    It is available with UDWorks and they can release it to you or modify it for you. Have you already contacted UDWorks and is there no response from them?

    Regards,

    Anshuman

  • Hello Anshuma,

    I  have contacted the UDWorks, they didn't provide me the code, and didn't tell me they could modify it for me.

    I think the web control code should be provided in RDK release package,  because the web control is a part of the DVR SYSTEM.

    Don't you think so?

     

    Thanks,

    Yanbin Yue

  • Hi,

    I am checking with UDWorks and get back to you soon on this.

     

    Regards,

    Anshuman

  • Hi Anshuman,

    OK, Waiting for your message.

     

    Thanks,

    Yanbin Yue

  • Hi,

    I have discussed this with UDWorks. Actually, the web server code is a single cab file which has details about their VMS source also. This is why, it is not included in the source package.

    Please contact Mr John Kim (john_kim@udworks.com). He would be able to provide the right direction by which either source code could be provided or UDWorks can help you to modify the binaries.

    Regards,

    Anshuman

    PS: Please mark this post as verified, if you think it has answered your question. Thanks.

  • HI, Anshuman,

    We have got their response before as following, but We think this is baffling. We could have not anything about VMS, but could not have the code of the WEB COTROL. The fact that they developed the VMS using source code like the WEB CONTROL doesn't as the cause the don't provide the WEB CONTROL source code, because the web control is a part of DVR, the costs of the DVR should have contained the cost of the WEB CONTROL source code.

    We need not they modify, because our application have a little complex, if we let them modify the binary, the cost will be large more.

    I think shouldn't develop the VMS for addtional profit.

    The UDWorks' response:

    ----------------------------------------------------------------------

    For the VMS code, unfortunately, it's not included the RDK package.

    That's why we just provide the sample program to test network streaming.

    To get it you have to make additional lincecse agreement with us and it will cost like below.

     

    Initial license : USD 1,200

    Running Royalty : USD 1.2 per chip

     

    Then, we will provide the SDK for VMS.

    ------------------------------------------------------------------

  • Hi,

    I propose that we can have a call and go over the path forward. May i know who is the local TI FAE and sales contact with whom you are interacting? I can work with him/her to setup a call and go over this issue to resolve it quickly. I would want to understand the exact requirement from your side, so that we can propose the best possible solution.

    Regards,

    Anshuman

  • Hi, Anshuman

    We don't have a  local TI FAE or sales. We bought the DVR directly from UDWorks, because we haven't found their sales in china.

    Could you let a local TI FAE in China contact us?My telephone number is +86 13453153267 or +86-0351-7035681-1023 and the email address is yybingyybing@foxmail.com. Our company is at Taiyuan Shanxi China.

     

    Thanks,

    Yanbin Yue