This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMIF clock on TMS320C6455 DSK

Other Parts Discussed in Thread: TMS320C6455

Hi,

I have a TMS320C6455 DSK kit from Spectrum Digital. I am trying to clock an external DAC with parallel input, and using Asynchronous EMIF write for that. I guess here are couple of the questions:

1. AECLKOUT which suppose to be used by EMIF cycle can be up to 166 MHz, which means with 2 cycle turn around time and 1 cycle for SETUP/STROBE/HOLD, the maximum clock (AWE) is 33.2 MHz. Am I correct, or there is any way to make it faster?

2. I am trying to make AECLKOUT to be 166 MHz, as a reference I am using pin 78 on Peripheral connector to measure output with oscilloscope. There is a lot of amiguity. SPRU971c, says the input clock is SYSCLOCK3, TMS320C6455 manual says it's SYSCLOCK4. I was able to change SYSCLOCK4 in GEL file, and see output at TP11 on DSK. However, ECLK_OUT pin 78 still has 96 MHz clock. What is wrong, or is there some sort of register I need to change? How to get that 166 MHz clock?

Thanks for any replies.

Vladimir

  • Vladimir Podosinov said:

    Hi,

    I have a TMS320C6455 DSK kit from Spectrum Digital. I am trying to clock an external DAC with parallel input, and using Asynchronous EMIF write for that. I guess here are couple of the questions:

    1. AECLKOUT which suppose to be used by EMIF cycle can be up to 166 MHz, which means with 2 cycle turn around time and 1 cycle for SETUP/STROBE/HOLD, the maximum clock (AWE) is 33.2 MHz. Am I correct, or there is any way to make it faster?

    166 MHz is the max clock speed.

    Vladimir Podosinov said:

    2. I am trying to make AECLKOUT to be 166 MHz, as a reference I am using pin 78 on Peripheral connector to measure output with oscilloscope. There is a lot of amiguity. SPRU971c, says the input clock is SYSCLOCK3, TMS320C6455 manual says it's SYSCLOCK4. I was able to change SYSCLOCK4 in GEL file, and see output at TP11 on DSK. However, ECLK_OUT pin 78 still has 96 MHz clock. What is wrong, or is there some sort of register I need to change? How to get that 166 MHz clock?

    Thanks for any replies.

    Vladimir

    Sorry, the datasheet is correct and the EMIF user guide is wrong.  You should use the AECLKINSEL bit to choose between SYSCLK4 and AECLKIN as the input clock to the EMIF.  Then set the PLLDIV4 value and make sure the divider is enabled.  If you're not seeing the value that you expect then perhaps your CPU frequency is also wrong (e.g. SYSREFCLK) or else one of your dividers is not programmed correctly.

  • Thanks for the help. It turned out that the AECLKINSEL bit was chosen to be an external clock, against my expectations. I tried to set it directly using CLS_FINST macro and just using plain integer pointer assignment, but did not sucseed. Is there any prerequisites to setting that bit?

  • Perhaps I misled you in my previous post.  The AECLKINSEL bit in the DEVSTAT register is a read-only bit.  Its value is based on the AEA15 pin at reset.  That pin has an internal pull-down so if you did not put an external pull-up then it will likely always come up as AECLKINSEL=0 (external clock).

  • Thanks again. I felt bad asking you question after I have found about DEVSTAT being read only, as I tried to keep changing that bit. Without hardware changes on the DSK board, is there a way to change that bit?

  • Sorry, it's only changeable through hardware.