Other Parts Discussed in Thread: OMAP3530
Hi all,
how can I configure DPLL4 in OMAP3530. In my design, it is configured to 864MHz, which is used as source clock for DSI PLL and PCLK. I need to configure PCLK to 74.25MHz to make use of HD feature. But with the current settings, PCLK is 72MHz. CM_CLKSEL2_PLL is the register in which we can set the multiplier and divider of DPLL4. But I need to know the formula or the source clock settings to produce the desired DPLL4 value.
Thanks,
Lakshmi.