This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK 2.0 and EDMA bw management



Hi,

I've got a very strange problem when i tried to integrate one of our signal processing apps with TI NDK:

forewords....

Our app is processing a 42Msamples/sec datastream coming from EMIFa with emifa bw of about 25%.

The deadline for transfers is very short.

We are using DSK6455 1GHz with a custom made FPGA daughtercard for data I/O

The CPU utilization is about 2.2%.

symptoms:

We've configured the NDK to use DHCP.

If I start the application, when actual packets are transmitted/received over the network

my EDMA transfers are badly slowed and it misses some data.

Is there a way to configure bus access priority between EDMA and EMAC DMA?

Am I pointing the finger in the wrong direction?? (maybe the ndk disables ints for

sometime or some other conflict?)

 

Best Regards

Max