This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMC6472 + using cache



Hello

I 'm trying to implement the H264 encoder on evmc6472 platform using CCS4 et BIOS5.

to reduce the encoding time of my project , I tried to add the memory cache using the CSL support.

in the build properties, in the include library file there is these libraries:  "liba.lib"     "csl_c6472.lib" and "csl_c64xplus_intc.lib".

I wrote in my code these instructions:

#include <csl.h>
#include <csl_dat.h>
#include <csl_cache.h>

void main(){

 

    CACHE_enableCaching(CACHE_EMIFA_CE00);
    CACHE_setL1pSize(CACHE_L1_32KCACHE);
    CACHE_setL1dSize(CACHE_L1_32KCACHE);
    CACHE_setL2Mode(CACHE_L2_NORMAL);
    CACHE_setL2Size(CACHE_256KCACHE);

....

func( );

....

}

The problem is that the encoding time was not reduced, as if it did not take into account the caches.

So please could someone tell me where is the problem? why it did not consider caches? I have to add additional instructions?

I 'll be very thankfull.

cordialy

David

  • David,

    I believe that BIOS5 has Cache Control built in.  You should just be able to do all of this from within your .tcf file and use the BCACHE APIs.  I don't know if the CSL APIs are compatible with Bios.

    See the BCACHE module section of http://www.ti.com/litv/pdf/spru403r

     

    Regards,

    Dan

     

  • David,

    In CCSv4, open the tcf file by double-clicking it in the Project window. Open the + on System then click on the Global Settings item. You will see the BIOS settings for cache below the middle of the list of settings in the center pane under "Global Settings properties" starting with 64P.... The default is 32k L1P cache, 32k L1D cache, and 0k L2 cache, and these will be used in the linker command file that BIOS generates. To change the L2 cache, right-click on Global Settings and select Properties, then change the L2 cache size on the 64PLUS tab to to 256k. This will add a section call CACHE_L2 to the MEM list, with base=0x00858000 and len=0x00040000. Click  the + on MEM under that, then click on LL2RAM to change its len from 0x00098000 to 0x00058000. Save the tcf and close it.

    You can now remove the CSL CACHE_* commands. BIOS will configure cache as described in the tcf and will do this before main() begins.

    You can use either the CSL CACHE_* commands or the BCACHE_* commands to make changes, but this is rarely the best way to do this. Using the tcf file integrates your changes into the linker command file and prevents code conflicts. As Dan said, the BCACHE_* are the better way to make changes, but even those are not advised for a cache configuration that you want to remain constant during the entire operation. Using other BCACHE_* commands for cache coherency operations is good, but you should not need to use CACHE_* or BCACHE_* for basic cache configuration.

    None of this explains your performance issues, but if you have conflicts between the linker command file and the CACHE_* configuration commands, you can have very bad problems in your application.

    Regards,
    RandyP

  •  thank you RandyP and Dan for your help

    I tried your suggestion. it's ok

    cordialy

    david

  • Hello RandyP

    after implementing my code on evmc6472 using a single core, I am trying to implement it on multiple cores, that why I started with a simple example that looks like the c6472_Edma_IPC_BIOS project.

      This is the summary of my example, I have two tasks where the first is effected by the core2 and it permits to fill two buffers: BUF 1 and BUF2 and then send an IPC to core3 to begin the second task responsible for filling a third buffer buf3 then sending an IPC to core2  to edit another time the buf3.

      this example is just to know how can communicate between cores.

    /*******************************************************************************************/

    #define size 20
    extern unsigned int SL2_Heap;
    unsigned char *buf1;
    unsigned char *buf2;
    unsigned char *buf3;
    void main()
    {

    .
    .
    //allocate three buffers in shared memory

    buf1 = (unsigned char*)MEM_calloc(SL2_Heap, sizeof(unsigned char)*size, 8);
    buf2 = (unsigned char*)MEM_calloc(SL2_Heap, sizeof(unsigned char)*size, 8); 
    buf3 = (unsigned char*)MEM_calloc(SL2_Heap, sizeof(unsigned char)*size, 8);
    IpcEventHook( 0, IPCIsr1 ); 
    IpcEventHook( 1, IPCIsr2 );
    .
    .
    }


    void TSK_Stage1_fnc(void)
    {
     int i;
        
     if ( CoreNum == 2 )
     {
      for(i=0;i<size;i++)
      {
       buf1[i]=2*i;
       buf2[i]=4*i;
       printf("buf1[%d] =%d  buf2[%d]=%d   \n",i,buf1[i],i,buf2[i]);
      }
      
      SetIpc( 3, 0 );  // send logical IPC to core 3
      
      SEM_pend( &SEM_Stage2, SYS_FOREVER );
      
      for(i=0;i<size;i++)
      {
       buf3[i]=buf3[i]>>1;
       printf("buf3[%d]=%d \n",i,buf3[i]);
      }
      for(i=0;i<size;i++)
     }
    }
     
    void TSK_Stage2_fnc(void)
    {
     int i;
     SEM_pend( &SEM_Stage1, SYS_FOREVER );  // wait for signal to start, from last core sending 1st data
     if ( CoreNum == 3 )
     {
      for(i=0;i<size;i++)
      {
       buf3[i]=i;
       printf("buf3[%d]=%d \n",i,buf3[i]);
      }
      SetIpc( 2, 1 );  // send logical IPC to core 2
     } 
    }
    // ISR for the IPC interrupt for logical IPC1, posts SEM_Stage1
    void IPCIsr1(void)
    {
     SEM_post( &SEM_Stage1 );
    }

    // ISR for the IPC interrupt for logical IPC2, posts SEM_Stage2
    void IPCIsr2(void)
    {
     SEM_post( &SEM_Stage2 );
    }

    /*************************************************************************/

    the problem I found is, when the core 3 sends an IPC to core 2, after calculating buf3, the Core 2 receives the IPC and normally it will make buf3 [i] = buf3 [i]>> 1;

      the problem was: the Core 2 did not use the new values ​​that are modified by core 3 in the task 2, but it uses the old values ​​which are zero although that all the three buffers are in shared memory.

      so how can I do to make the core 2 uses the new values ​​of buf3. and can you tell me if there are other problems in my example.

    I will be very thankfull.

    Cordialy

    david
     


     

  • David,

    Since this is marked Answered, you may not get many support views. If my answer is not sufficient, you may want to post this as a new thread. You can offer a link back to this thread if it makes it easier.

    Cache coherency.

    Set a breakpoint on each processor after the SEM_pend's, then look at the buffers in a memory window before and after the processing loops. Especially observe any color coding that shows values stored in cache. Then you may want to halt another processor and observe the same buffers from its point-of-view.

    What do you find, or is this debug technique helpful at all?

    Regards,
    RandyP

     

    If you need more help, please reply back. If this answers the question, please click  Verify Answer  , below.