Other Parts Discussed in Thread: OMAP-L137
Hi.
I'm currently testing the AER Librairies on OMAP-L137 EVM with a home-made audio Expansion Board.
Audio are sampled at 16 kHz, but Echo Cancellation seems to work only with 0-4KHz signal.
I read In the Quick Tuning Guide : " If AER is running at 16kHz, configure AER such that high band is dropped for both Tx
and Rx paths by setting bits aer_CTL1_DROP_TX_HIGH_BAND and
aer_CTL1_DROP_RX_HIGH_BAND respectively."
Should I conclude that Echo Cancellation can not work on the 4KHz-8KHz frequency band ?