This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM57X: PROCESSOR-SDK-AM57X

Part Number: PROCESSOR-SDK-AM57X


Hello,

I am having an issue much the same as in the related thread.

When attempting to run any gstreamer pipelines on the AM57X in linux, I get the following:

gst-launch-1.0 filesrc location=/test.yuv ! videoparse width=352 height=288 format=nv12 ! queue ! ducatih264enc ! h264parse ! queue ! ducatih264dec
Setting pipeline to PAUSED ...
[ 303.833017] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
MmRpc_create: Error: connect failed
ERROR: Pipeline doesn't want to pause.
../git/libdce.c:416: dce_ipc_init ERROR: Failed eError == DCE_EOK error val -4../git/libdce.c:479: Engine_open ERROR: Failed dce_ipc_init(coreIdx) == DCE_EOK error val -4Setting pipeline to NULL ...
Freeing pipeline ...

The related thread indicated that in his/her case, that  /dev/rpmsg-dce was not created.  In my case, however, that device does exist.  I checked the resource table/config file and compared the memory map to what is in my device tree, and that matched:

ipu2_cma_pool: ipu2_cma@9B800000 {
compatible = "shared-dma-pool";
reg = <0x0 0x9B800000 0x0 0x3800000>;
// size = <0x0 0x3800000>;
reusable;
status = "okay";
};

#define PHYS_MEM_IPC_VRING      0x9B800000

9500_0000 9500_0000 6_0000 ( 384 kB) TRACE_BUF
9506_0000 9506_0000 1_0000 ( 64 kB) EXC_DATA
9507_0000 9507_0000 2_0000 ( 128 kB) PM_DATA (Power mgmt)

TRACE_BUF: { name: "TRACE_BUF", base: 0x95000000, len: 0x00060000, space: "data", access: "RW" },
EXC_DATA: { name: "EXC_DATA", base: 0x95060000, len: 0x00010000, space: "data", access: "RW" },

PM_DATA: { name: "PM_DATA", base: 0x95070000, len: 0x00020000, space: "data", access: "RWX" }

Are there any other ideas of what to look at here?