While executing the single camera application using AR0233 camera sensor module over Jacinto 7 EVM board interfaced with fusion board (Jacinto EVM-FusionBoard-AR0233),
faced the below errors, PFA the snapshot for the same.
Errors log:
Display Set Target done
vxSeraphScheduleConfig done
59.253246 s: VX_ZONE_ERROR:[ownCtextSendCmd:814] Command ack message returned failure cmd_status: -1
59.253286 s: VX_ZONE_ERROR:[ownConxtSendCmd:850] tivxEventWait() failed.
59.253293 s: VX_ZONE_ERROR:[ownNodeKernelInit:538] Target kernel, TIVX_CMD_NODE_CREATE failed for node node_95
59.253299 s: VX_ZONE_ERROR:[ownNodeKernelInit:539] Please be sure the target callbac have been registered for this core
59.253305 s: VX_ZONE_ERROR:[ownNodeKernelInit:540] If the target callbacks ha been registered, please ensure no errors are occurring withinhe create callback of l
59.253463 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 0kernel com.ti.capture ... failed !!!
59.253477 s: VX_ZONE_ERROR:[vxVerifyGraph:2055] Node kernel init failed
59.253482 s: VX_ZONE_ERROR:[vxVerifyGraph:2109] Graph verify fled
Scaler is enabled
So could anyone help to resolve this error, or suggest the required code changes from single camera application or driver point of view