Part Number: AM625
Hi experts
1.The touch panel is an I2C interface. Which I2C is the best way to connect? And about touch interrupt, is it possible to use pin A15?
2.LCD backlight dim control, which IO should be used to output PWM? Can the C13 pin of the AM6254 be used?
Currently unused ePWM pins are: B14, C13, A13, A14, B18, B13, E18.
3.The external GPS module is a serial port interface. Which one of the following two serial ports is better?
MCU_UART0
WKUP_UART0
BR
Ethan