This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Maximum Current Ratings at Power Terminals in AM62x datasheet

Genius 13655 points
Part Number: AM625


Hello Champs,

Customer needs the maximum current ratings info at power terminals for each power rail, there is no such info in datasheet, especially for VDDSHV_MCU,VDDA_MCU,DVDDSHV_MMCx pins. Could you provide this info like below am335x. 


Thanks.
Rgds
Shine

  • Hello Shine,

    Thank you for the Query.

    We have a similar thread that has been answered. 

    Please refer below

    AM625: Power consumption of AM625 - Processors forum - Processors - TI E2E support forums

    And refer below table for Power supply names

    VDD_CORE

    VDD_CORE, VDDA_CORE_CSIRX0, VDDA_CORE_USB, VDDA_DDR_PLL0, VDD_CANUART

    VDDR_CORE   

    VDDR_CORE

    VDDS_DDR

    VDDS_DDR, VDDS_DDR_C

    1.8V Analog

    VDDA_PLL0, VDDA_PLL1, VDDA_PLL2, VDDA_1P8_CSIRX0, VDDA_1P8_OLDI0, VDDA_1P8_USB, VDDA_TEMP0, VDDA_TEMP1, VDDS_OSC0

    1.8 VDDSHVx 

    VDDSHV0 to VDDSHV6, VMON_1P8_SOC, VDDSHV_CANUART (if powering with 1.8V)

    3.3V VDDSHVx 

    VDDSHV0 to VDDSHV6, VMON_3P3_SOC, VDDA_3P3_USB, VDDSHV_CANUART (if powering with 3.3V)

    SD IF

    VDDSHV5 (SoC_VDDSHV5_SDIO(MMC1))

    1.8V MCU Analog

    VDDA_MCU

    3.3V MCU IO     

    VDDSHV_MCU

    Efuse VPP          

    VPP

    Please let me know if you have any additional questions.

    Regards,

    Lavanya M R.