Part Number: TDA4VM-Q1
Hi team,
Here're some questions from the customer may need your help:
Regarding the development of TDA4AL, the customer has following questions:
1) Is the OTP user side inside the HS chip readable? Or is it controlled entirely by DMSC and not visible to the user side?
2) Does the chip ID refer to the value in the registers? Is the ID separate and unique per TDA4? And the corresponding address bits in the TRM are 4300 0020h~4300 002Ch?
3) Customer wants to use TDA4 to provide a dual-eye camera for external trigger signals (Triggers) and to be able to precisely adjust the delay between two trigger signals, preferably at the us level.
Is it required to connect the trigger signal to an IO that supports the timer? If so, should it be placed on timer in the MCU domain or timer in the main domain?
4) Is there a power evaluation tool for the chip? For example, evaluate the approximate current value of each circuit.
5) Is there a hardware design checklist?
Could you help check this case? Thanks.
Best Regards,
Cherry