Part Number: SK-AM64B
Other Parts Discussed in Thread: UNIFLASH
My customer is seeing the following issues when trying to get started with R5F development on the SK-AM64B EVM.
- UART boot started kinda working – but ends in XMODEM send failed in Python script
- See image below
- Tried many times on 2 different boards. Never works but gets different data every time.
- SOC Initialization Using SD Boot provides no visual indication that its working
- Maybe it did something, Im not sure, because UART boot wasn’t printing “C” but now it is after I tried booting with that SD card.
- SOC Initialization Using CCS Scripting doesn’t work
- Cant get past this error -1170
- Have tried connecting JTAG after powering on
- But I can connect to the PRUs, see image below
- Cant get past this error -1170
Is “mcu_plus_sdk_am64x_08_04_00_17” the right version to be using with SK-AM64B ?
UART boot problem :

PRU Connection works but M3 connection does not :