Hi experts,
My sdk version is 08_04_00_06 with sdl in it.I'm running sdl/example/ecc_ app and I have some questions.
>>In Software Diagnostics Library (SDL) - J721E User Guide 01_00_00, it shows UC-1 and UC-2 are Wrapper type and UC-3 are Interconnect type,
but in sdlr_soc_ecc_aggr.h , all of them are Interconnect type as shown below
#define SDL_COMPUTE_CLUSTER0_MSMC_ECC_AGGR0_CLEC_J7ES_CLEC_EDC_CTRL_BUSECC_ECC_TYPE (1U)
#define SDL_COMPUTE_CLUSTER0_MSMC_ECC_AGGR0_MSMC_MMR_BUSECC_ECC_TYPE (1U)
#define SDL_COMPUTE_CLUSTER0_MSMC_ECC_AGGR0_VBUSP_CFG_DSP4_P2P_DST_BUSECC_ECC_TYPE (1U)
Which is correct?
>>How to inject an error for wapperer type RAM e.g.SDL_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR_MCANSS_MSGMEM_WRAP_MSGMEM_ECC_RAM_ID?
I modified the code referring to the example ecc_app, the interconnect type SEC error can be received normally, but the wrapper type cannot.
Thanks,
Shukai