Part Number: TDA4VM
Other Parts Discussed in Thread: SYSBIOS
We had a stuck A72 issue:
The serial output information is as follows:
ERROR: Unhandled External Abort received on 0x80000001 from S-EL1
ERROR: exception reason=0 syndrome=0xbf000000
Unhandled Exception from EL1
x0 = 0x0000021ca06ea007
x1 = 0x000000000000710c
x2 = 0xffff8000112fec50
x3 = 0x0000000000000000
x4 = 0x0000000000000000
x5 = 0xffff00087fa81848
x6 = 0x0000000000000258
x7 = 0xffff800010594898
x8 = 0xffff8000110c7000
x9 = 0x3a676e69636e7973
x10 = 0x702d6b6361747320
x11 = 0x726f746365746f72
x12 = 0x6c656e72654b203a
x13 = 0x69206b6361747320
x14 = 0x707572726f632073
x15 = 0xffff00080de76728
x16 = 0x0000000000000000
x17 = 0x0000000000000000
x18 = 0x0000000000000010
x19 = 0xffff8000110609d8
x20 = 0x0000000000030d41
x21 = 0x0000021ca06e7d1b
x22 = 0xfffffde35f91d105
x23 = 0x0000000000000044
x24 = 0x0000000000418958
x25 = 0xffff8000109bf178
x26 = 0xffff800011a21db0
x27 = 0xffff00080de76838
x28 = 0xffff800019fcfb08
x29 = 0xffff800019fcf970
x30 = 0xffff800010999e20
scr_el3 = 0x000000000000073d
sctlr_el3 = 0x0000000030cd183f
cptr_el3 = 0x0000000000000000
tcr_el3 = 0x0000000080803520
daif = 0x00000000000002c0
mair_el3 = 0x00000000004404ff
spsr_el3 = 0x0000000080000005
elr_el3 = 0xffff800010999e18
ttbr0_el3 = 0x0000000070010b00
esr_el3 = 0x00000000bf000000
far_el3 = 0x0000000000000000
spsr_el1 = 0x0000000080000005
elr_el1 = 0xffff800010999e18
spsr_abt = 0x0000000000000000
spsr_und = 0x0000000000000000
spsr_irq = 0x0000000000000000
spsr_fiq = 0x0000000000000000
sctlr_el1 = 0x0000000034d4d91d
actlr_el1 = 0x0000000000000000
cpacr_el1 = 0x0000000000300000
csselr_el1 = 0x0000000000000000
sp_el1 = 0xffff800019fcf970
esr_el1 = 0x0000000056000000
ttbr0_el1 = 0x000000088abbe800
ttbr1_el1 = 0x0400000080e10000
mair_el1 = 0x0000bbff440c0400
amair_el1 = 0x0000000000000000
tcr_el1 = 0x00000034f5d07590
tpidr_el1 = 0xffff80086ebe0000
tpidr_el0 = 0x0000ffff57b8f890
tpidrro_el0 = 0x0000000000000000
par_el1 = 0x0000000000000000
mpidr_el1 = 0x0000000080000001
afsr0_el1 = 0x0000000000000000
afsr1_el1 = 0x0000000000000000
contextidr_el1 = 0x0000000000000000
vbar_el1 = 0xffff800010081800
cntp_ctl_el0 = 0x0000000000000005
cntp_cval_el0 = 0x0000021cf2424a9e
cntv_ctl_el0 = 0x0000000000000000
cntv_cval_el0 = 0x0000000000000000
cntkctl_el1 = 0x00000000000000d6
sp_el0 = 0x000000007000abd0
isr_el1 = 0x0000000000000040
dacr32_el2 = 0x0000000000000000
ifsr32_el2 = 0x0000000000000000
cpuectlr_el1 = 0x0000001b00000040
cpumerrsr_el1 = 0x0000000000000000
l2merrsr_el1 = 0x0000000000000000
use trace32 attach to a72 get the stack frame:
cpu0 in die:

cpu1 in panic: