This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dm684 + Need help



Hello

I am working on dm648 , i have modified the HelloWorld project so as the ethernet subsystem is configured in ALE bypass mode .

Once i done tht the performance of the board has greatly decreased. If the too much load/ traffic is flooded on the board it halts after some time . And no packets are sent or received.

I know in ALE bypass mode , the packets coming to board via Port 0 and Port 1 are first routed to dsp (Port2 ) and then routed to desired ethernet physical ports. So dsp is involved in each packet being received either a broadcast packet is received or a non-broadcast packet is received. I know it will introduce some delays ... but can u help in setting the value of register to best values so that performance doesnt decreased?? plz need help

Second the throughput documents tht i have found on net , does not tell about the mode of information meaning whether the board was in ALE bypass mode or normal mode.
Kindly tell me wht is maximum throughput attainable in ALE by pass mode.

The etherent subsystem module document speaks only a little about ALE bypass mode , kindly send me more informattion on it.

Thank you for ur time
Looking forward to ur reply
Regards
Amna