Part Number: AM5728
Other Parts Discussed in Thread: PMP
Hi,
As per the SDK developer guide to build the minimal filesystem using arago-base-tisdk-image.
I am following the link:
1. Overview — Processor SDK Linux Documentation
facing the below bitbake error:
icsandroid@icsandroid-Latitude-E5520:~/tisdk/build$ MACHINE=am57xx-evm bitbake tisdk-rootfs-image
Loading cache: 100% |############################################| Time: 0:00:00
Loaded 3257 entries from dependency cache.
Parsing recipes: 100% |##########################################| Time: 0:00:01
Parsing of 2509 .bb files complete (2508 cached, 1 parsed). 3257 targets, 499 skipped, 0 masked, 0 errors.
WARNING: No recipes available for:
/home/icsandroid/tisdk/sources/meta-openamp/recipes-bsp/device-tree/device-tree-generation_%.bbappend
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.32.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am57xx-evm"
DISTRO = "arago"
DISTRO_VERSION = "2017.06"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:2b7f7b00654eb3faaea7c66271ebe508b9ffc019"
meta-arago-distro
meta-arago-extras = "HEAD:8f49ed67d0627a04ac72fd388fda7756273ba2d7"
meta-browser = "HEAD:08576b03af624b65ad949c410d84c11c7d1f2e39"
meta-openamp = "HEAD:8a214032bfb7e8124bc1485c70c69f7d60abb819"
meta-qt5 = "HEAD:2c9f0e4eb0e9097f6f872ec1e1d81768a8ab5f1b"
meta-networking
meta-ruby
meta-python
meta-oe
meta-gnome = "HEAD:fe5c83312de11e80b85680ef237f8acb04b4b26e"
meta-ti = "HEAD:a18d57af8384ced25996739bb66d197c69efb77b"
meta-linaro-toolchain
meta-optee = "HEAD:49b0f32d7e955f250b0022d1b2f403f45a2c2d9c"
meta = "HEAD:e3911133ee9aad7cc3ae89faea80a097f6614fab"
Initialising tasks: 100% |#######################################| Time: 0:00:22
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: qtbase-native-5.7.1+gitAUTOINC+a55f36211e-r0 do_fetch: Failed to fetch URL git://github.com/qtproject/qtbase.git;name=qtbase;branch=5.7;protocol=git, attempting MIRRORS if available
WARNING: qtxmlpatterns-5.7.1+gitAUTOINC+89dbcc4f80-r0 do_fetch: Failed to fetch URL git://github.com/qtproject/qtxmlpatterns.git;name=qtxmlpatterns;branch=5.7;protocol=git, attempting MIRRORS if available
ERROR: qtxmlpatterns-5.7.1+gitAUTOINC+89dbcc4f80-r0 do_fetch: Fetcher failure: Fetch command export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-CP8mYz0Nn7"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/icsandroid/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/qt5:/home/icsandroid/tisdk/sources/oe-core/scripts:/home/icsandroid/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/arm-linux-gnueabi:/home/icsandroid/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/am57xx-evm/usr/bin/crossscripts:/home/icsandroid/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin:/home/icsandroid/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/icsandroid/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin:/home/icsandroid/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/bin:/home/icsandroid/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/icsandroid/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/icsandroid/tisdk/sources/meta-browser/scripts:/home/icsandroid/tisdk/sources/oe-core/scripts:/home/icsandroid/tisdk/sources/bitbake/bin:/home/icsandroid/bin:/home/icsandroid/.local/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/icsandroid"; LANG=C git -c core.fsyncobjectfiles=0 fetch -f --prune --progress git://github.com/qtproject/qtxmlpatterns.git refs/*:refs/* failed with exit code 128, output:
fatal: I don't handle protocol '“https'
ERROR: qtxmlpatterns-5.7.1+gitAUTOINC+89dbcc4f80-r0 do_fetch: Fetcher failure for URL: 'git://github.com/qtproject/qtxmlpatterns.git;name=qtxmlpatterns;branch=5.7;protocol=git'. Unable to fetch URL from any source.
ERROR: qtxmlpatterns-5.7.1+gitAUTOINC+89dbcc4f80-r0 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/icsandroid/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtxmlpatterns/5.7.1+gitAUTOINC+89dbcc4f80-r0/temp/log.do_fetch.2206
ERROR: Task (/home/icsandroid/tisdk/sources/meta-qt5/recipes-qt/qt5/qtxmlpatterns_git.bb:do_fetch) failed with exit code '1'
Need help.
Thanks and regards,
AfrinBanu