Hi, TI,
The encode drive(wave5.ko) of TDA4VECO requires cma memory. We successfully applied for a piece of cma memory in the high 32-bit address space, with a size of 512M(addr = 0x8 9000 0000, size = 0x2000 0000).
No error occurred during the loading of the drive.
But errors will occur when we call the following interface.

The following error occurred

Whether encode driver can use high 32-bit memory?How do I need to modify it if I can.
Best Regards
Alex