This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP L138 DDR2 Controller

I am working on board with an OMAP L138 connected to a DDR. I am using the gel script for configuring the ddr controller. I think it is set up correctly except that I have one issue. If I write to a memory location, I cannot read back from the same location until I repeat the read command multiple times. So if I write to one location and read from that location multiple times, I see that every 4th read iteration yields the data that I wrote. Below is my gel script along with a link to the DDR2 memory I am using. I am running at a clock rate of 150MHz.

Link to DDR2 Memory

http://download.micron.com/pdf/datasheets/dram/ddr2/512MbDDR2.pdf

 

Any help is appreciated.

 

DEVICE_DDRConfig(unsigned int freq)

{

GEL_TextOut("\t\t\tDDR initialization entering DDRConfig()....\n","Output",1,1,1);

/*Enable the Clock to EMIF3A SDRAM*/

PSC1_LPSC_enable(PD0, LPSC_DDR);

 

/*If VTP caliberation enabled , then skip the VTP calibration*/

if((VTPIO_CTL & 0x00000040))

{

// Begin VTP Calibration

VTPIO_CTL |= (0x00004000); // Set IOPWRDN bit to enable input buffer powerdown enable mode

VTPIO_CTL &= ~(0x00000040); // Clear POWERDN bit (enable VTP)

 

// Pulse (low) CLRZ to initiate VTP IO Calibration

VTPIO_CTL |= (0x00002000); // Set CLRZ bit

VTPIO_CTL &= ~(0x00002000); // Clear CLRZ bit (CLRZ should be low for at least 2ns)

VTPIO_CTL |= 0x00002000; // Set CLRZ bit

 

// Polling READY bit to see when VTP calibration is done

while(!((VTPIO_CTL & 0x00008000)>>15)) {}

 

VTPIO_CTL |= 0x00000080; // Set LOCK bit for static mode

VTPIO_CTL |= 0x00000100; // Set PWRSAVE bit to save power

VTPIO_CTL |= 0x00000040; // Set POWERDN bit to power down VTP module

// End VTP Calibration

}

 

EMIF3A_SDCR |= 0x00800000; // Set BOOTUNLOCK

 

// **********************************************************************************************

// Setting based on MT47H32M16 – 8 Meg x 16 x 4 banks

// Config DDR timings

GEL_TextOut("\t\t\tStarting DDRCTL Config....\n","Output",1,1,1);

DDRCTL = (0x0 << 8) | // Reserved

(0x1 << 7) | // EXT_STRBEN

(0x1 << 6) | // PWRDNEN

(0x0 << 3) | // Reserved

(0x4 << 0); // RL

GEL_TextOut("\t\t\tStarting EMIF3A_SDCR Config....\n","Output",1,1,1);

EMIF3A_SDCR = (EMIF3A_SDCR & 0xF0000000) | // Reserved

(0x0 << 27) | // DDR2TERM1

(0x1 << 26) | // IBANK_POS

(0x0 << 25) | // MSDRAMEN

(0x0 << 24) | // DDRDRIVE1

(0x0 << 23) | // BOOTUNLOCK

(0x0 << 22) | // DDR2DDQS

(0x0 << 21) | // DDR2TERM0

(0x1 << 20) | // DDR2EN

(0x0 << 19) | // DDRDLL_DIS

(0x1 << 18) | // DDRDRIVE0

(0x1 << 17) | // DDREN

(0x1 << 16) | // SDRAMEN

(0x1 << 15) | // TIMUNLOCK

(0x1 << 14) | // NM

(0x0 << 12) | // Reserved

(0x5 << 9) | // CL //CL=5 Based on DDR

(0x0 << 7) | // Reserved

(0x2 << 4) | // IBANK

(0x0 << 3) | // Reserved

(0x2 << 0); // PAGESIZE

 

GEL_TextOut("\t\t\tStarting EMIF3A_SDTIMR1 Config....\n","Output",1,1,1);

// Subtracting 0.5 instead of 1 so that the int is rounded up after truncating a real value

EMIF3A_SDTIMR1 = (((unsigned int) ((105.0 * freq / 1000) - 1)) << 25)| // tRFC

(((unsigned int) ((12.5 * freq / 1000) - 1)) << 22) | // tRP

(((unsigned int) ((12.5 * freq / 1000) - 1)) << 19) | // tRCD

(((unsigned int) ((15.0 * freq / 1000) - 1)) << 16) | // tWR

(((unsigned int) ((40.0 * freq / 1000) - 1)) << 11) | // tRAS

(((unsigned int) ((55.0 * freq / 1000) - 1)) << 6) | // tRC

(((unsigned int) ((7.5 * freq / 1000) - 1)) << 3) | // tRRD

(EMIF3A_SDTIMR1 & 0x4) | // Reserved

(((unsigned int) ((7.5 * freq / 1000) - 1)) << 0); // tWTR

 

// Subtracting 0.5 instead of 1 so that the int is rounded up after truncating a real value

// tRASMAX is rounded down so subtracting 1

// CAS/CL = 3

 

GEL_TextOut("\t\t\tStarting EMIF3A_SDTIMR2 Config....\n","Output",1,1,1);

EMIF3A_SDTIMR2 = (EMIF3A_SDTIMR2 & 0x80000000) | // Reserved

(((unsigned int) ((70000 / 7812.5) - 1)) << 27) | // tRASMAX [(70us/7.8125us)-1]

(0x2 << 25) | // tXP //Check what value this should be -MS

(0x0 << 23) | // tODT (Not supported)

(((unsigned int) ((115.0 * freq / 1000) - 1)) << 16) | // tXSNR

((200 - 1) << 8) | // tXSRD (200 Cycles) -MS

((1 - 1) << 5) | // tRTP (1 Cycle) -MS

(0x2 << 0); // tCKE //min 3 -MS

 

GEL_TextOut("\t\t\tStarting EMIF3A_SDCR Config....\n","Output",1,1,1);

 

EMIF3A_SDCR &= ~0x00008000; // Clear TIMUNLOCK

 

GEL_TextOut("\t\t\tStarting EMIF3A_SDCR2 Config....\n","Output",1,1,1);

//EMIF3A_SDCR2 = 0x00000004; // IBANK_POS set to 0 so this register does not apply

EMIF3A_SDCR2 = (0x4 << 0) | // 13 row address lines

(0x0 << 16); // 4 banks will be refreshed

 

 

EMIF3A_SDRCR = (0x1 << 31) | // LPMODEN

(0x1 << 30) | // MCLKSTOPEN

(0x0 << 24) | // Reserved

(0x1 << 23) | // SR_PD

(0x0 << 16) | // Reserved

(((unsigned int) ((7.8125 * freq))) << 0); // RR

 

GEL_TextOut("\t\t\tReady to SyncReset the Clock to EMIF3A SDRAM....\n","Output",1,1,1);

/*SyncReset the Clock to EMIF3A SDRAM*/

PSC1_LPSC_SyncReset(PD0, LPSC_DDR);

 

GEL_TextOut("\t\t\tReady to Enable the Clock to EMIF3A SDRAM....\n","Output",1,1,1);

/*Enable the Clock to EMIF3A SDRAM*/

PSC1_LPSC_enable(PD0, LPSC_DDR);

 

EMIF3A_SDRCR &= ~0xC0000000; // disable self-refresh

GEL_TextOut("\t\t\tCompleted Configuration of all DDR2 registers....\n","Output",1,1,1);

}

 

 

Link to DDR2 memory

 

-Manas