Hi,
I am trying to simply use EDMA to transfer data from DDR to on-chip memory, and I am a bit stuck. I believe the PaRAM set is properly configured with the correct source and destination addresses, and the channel is configured to use that PaRAM set, but as soon as I trigger the channel I get the EMR showing a missed event, and the TC ERRSTAT register showing MMRAERR ("User attempted to read or write to an invalid address in configuration memory map."). I can write to or read from the same addresses as submitted for the transfer if I do it manually. Anyone have hints as to how to proceed here or what I may be doing wrong?
Many thanks,
B.