This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 EVM board McASP "XCKFAIL" error?

Hi,

I am getting an "XCKFAIL" error once upon I enable the McASP 0 clock by using following: 

WR_MEM_32(CM_ALWON_L3_SLOW_CLKSTCTRL, 2);  /* 0x48181400 = 2*/

WR_MEM_32(CM_ALWON_MCASP_0_CLKCTRL, 2);  /* 0x48181540 = 2*/

The McASP transmit status XSTAT never has XDATA ready (=0)  status.

Can somebody tell me what else I should have configured to make the McASP clock working?

 

Thanks in advance.

Philip

 

  • Hi Philip,

    Please post your query at DaVinci Video Processor section of the e2e community. For your reference, link is given below.

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/default.aspx

     

    Regards,

    Ankit Agrawal

  • Hi Philip,

    It appears from the code that you are starting the clocks, do you have the McASP module itself enabled? Are there any pinmux items that could be affecting it? Do you have all the other transmit parameters configured?

    Regards,

    Viet