Hello ;
I working on dm648 , the board is connected to lan and PC by rj45 jacks...
In normal mode , the LAN activity is great such that you can configure outlook and send mails of varying sizes and ping any pc on the network.
But when i configured my board in ALE bypass mode , things run fine meaning the LAN activity is okay ... but with time it keeps on degrading ... Such that Once the Microsoft Outlook connection is lost it is not established again and the ping responses dont come ....
Wht is causing the problem i am not sure , i hve build up my code on "helloWorld" project which came with NDK version 1.92.
I hve taken all the right steps in configuring the board to ALE bypass mode...
Kindly plz guide as to wht is causing the pb with troughput of the board.... how can i increase the performance...
Waiting for a reply
Regards
Amna