Other Parts Discussed in Thread: AM1707
Hi,
1. Could I use IAR Embedded workbench IDE 5.3 with JLink to debug and download the code to AM1707? Because IAR it support ARM926EJ-S, I thought it could work appropriately just to modify linker command file, but it didn't work. I don't know if it can really work as I thought, if it is, could somebody tell me what exactly the procedure is?
2. Does AM1707 provide the way to access the local ROM when it is just manufactured? I know that it provide a lot of ways to boot, but I wonder that if I can download code without any extra facilities( such as JLink )?