This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM64X: AM64 HS-FS git brah

Part Number: PROCESSOR-SDK-AM64X


In this Doc,

/AM64x-Processor-SDK-08_04_01_04-Documentation/0_04_01_04/linux/Foundational_Components/U-Boot/UG-General-Info.html#build-u-boot

There are 5 parts:

I have checked out all of them, but the branches I saw are not matching the version numbers shown in this doc.

Please post the correct git commands.

I don't want to try and error for miss-using the wrong versions numbers.

BR Rio

  • Hello Rio,
    These're git repositories to "repo" source instead of using SDK package.
    For example, I'm able to repo, and checkout u-boot source matching SDK 8.4 with the tag "08.04.01.005" as noted in the SDK release note.

    I have checked out all of them, but the branches I saw are not matching the version numbers shown in this doc.

    Will you elaborate the above comments?

    Best,
    -Hong