Other Parts Discussed in Thread: DM3730
Hi all
I am trying to build a training application for Cortex A8 and using Code Sourcery Lite version tool chain on DM3730 with PowerVR SGM and the application using libEGL library which is installed at LIBDIR directory. But there is an error when I type "make PLATFORM=LinuxOMAP3" according to "OpenGL ES 2.x SDK User Guide". The output is below:
Thanks in advance.
- Volkan
------------------------------
volkan@volkan-desktop:~/OMAP35x_Graphics_SDK_3_01_00_06/GFX_Linux_SDK/OGLES2/SDKPackage/TrainingCourse/01_Initialization/OGLES2/Build/LinuxOMAP3$ make PLATFORM=LinuxOMAP3
mkdir -p ../LinuxOMAP3/ReleaseRaw
arm-none-linux-gnueabi-g++ -o ../LinuxOMAP3/ReleaseRaw/OGLES2Initialization ../LinuxOMAP3/ReleaseRaw/OGLES2Initialization_NullWS.o -lEGL -lGLESv2
/home/volkan/CodeSourcery/Sourcery_G++_Lite/bin/../lib/gcc/arm-none-linux-gnueabi/4.3.3/../../../../arm-none-linux-gnueabi/bin/ld: cannot find -lEGL
collect2: ld returned 1 exit status
make: *** [../LinuxOMAP3/ReleaseRaw/OGLES2Initialization] Error 1
volkan@volkan-desktop:~/OMAP35x_Graphics_SDK_3_01_00_06/GFX_Linux_SDK/OGLES2/SDKPackage/TrainingCourse/01_Initialization/OGLES2/Build/LinuxOMAP3$
------------------------------
(export LIBDIR="/home/volkan/OMAP35x_Graphics_SDK_3_01_00_06/GFX_Linux_SDK/OGLES2/SDKPackage/Builds/OGLES2/LinuxOMAP3/lib:${LIBDIR}")