Part Number: AM6548
Dear TI,
We have an LVDS Screen connected to our custom baseboard with the TI AM6548 Processor. The performance when displaying applications such as kmscube is very poor. Additional details below:
- Kmscube reports that it is operating at about 5 FPS:
root@tqma65xx-2gb-mba65xx:~# kmscube MESA-LOADER: failed to open tidss: /usr/lib/dri/tidss_dri.so: cannot open shared object file: No such file or directory (search p$ failed to load driver: tidss Using display 0xaaaae94f29b0 with EGL version 1.4 =================================== EGL information: version: "1.4" vendor: "Mesa Project" client extensions: "EGL_EXT_client_extensions EGL_EXT_device_base EGL_EXT_device_enumeration EGL_EXT_device_query EGL_EXT_platf$ display extensions: "EGL_ANDROID_blob_cache EGL_EXT_buffer_age EGL_EXT_image_dma_buf_import EGL_EXT_image_dma_buf_import_modifi$ =================================== OpenGL ES 2.x information: version: "OpenGL ES 3.1 Mesa 21.0.3" shading language version: "OpenGL ES GLSL ES 3.10" vendor: "Mesa/X.org" renderer: "softpipe" extensions: "GL_EXT_blend_minmax GL_EXT_multi_draw_arrays GL_EXT_texture_filter_anisotropic GL_EXT_texture_compression_s3tc GL_$ =================================== Using modifier ffffffffffffff Modifiers failed! Using modifier ffffffffffffff Modifiers failed! Rendered 10 frames in 2.050202 sec (4.877568 fps) Rendered 20 frames in 4.117058 sec (4.857838 fps) Rendered 30 frames in 6.142262 sec (4.884194 fps) Rendered 40 frames in 8.150817 sec (4.907483 fps) Rendered 50 frames in 10.176011 sec (4.913517 fps)
- Kmstest isn't able to find any drm drivers:
root@tqma65xx-2gb-mba65xx:~# kmstest trying to open device 'i915'...failed trying to open device 'amdgpu'...failed trying to open device 'radeon'...failed trying to open device 'nouveau'...failed trying to open device 'vmwgfx'...failed trying to open device 'omapdrm'...failed trying to open device 'exynos'...failed trying to open device 'tilcdc'...failed trying to open device 'msm'...failed trying to open device 'sti'...failed trying to open device 'tegra'...failed trying to open device 'imx-drm'...failed trying to open device 'rockchip'...failed trying to open device 'atmel-hlcdc'...failed trying to open device 'fsl-dcu-drm'...failed trying to open device 'vc4'...failed trying to open device 'virtio_gpu'...failed trying to open device 'mediatek'...failed trying to open device 'meson'...failed trying to open device 'pl111'...failed trying to open device 'stm'...failed trying to open device 'sun4i-drm'...failed trying to open device 'armada-drm'...failed trying to open device 'komeda'...failed trying to open device 'imx-dcss'...failed no device found main: Could not open device (No such device) root@tqma65xx-2gb-mba65xx:~#
- Running a simple Qt QML Application with EGLFS using the eglfs_kms integration is pretty slow as well. I believe eglfs_kms relies on hardware acceleration (GPU). Correct me if I'm wrong.
- For the TI AM6548, I believe the DRM driver is the tidss. Should kmstest be able to find this? I can confirm that the tidss kernel module is loaded with the lsmod command:
root@tqma65xx-2gb-mba65xx:~# lsmod Module Size Used by hid_multitouch 327680 0 usbhid 327680 0 xhci_plat_hcd 327680 0 xhci_hcd 393216 1 xhci_plat_hcd usbcore 458752 3 xhci_hcd,usbhid,xhci_plat_hcd dwc3 327680 0 udc_core 262144 1 dwc3 usb_common 262144 5 xhci_hcd,usbcore,xhci_plat_hcd,dwc3,udc_core crct10dif_ce 262144 1 tidss 327680 0 videobuf2_dma_contig 262144 1 tidss videobuf2_memops 262144 1 videobuf2_dma_contig phy_omap_usb2 262144 4 v4l2_mem2mem 262144 1 tidss dwc3_keystone 262144 0 videobuf2_v4l2 262144 2 tidss,v4l2_mem2mem videobuf2_common 327680 3 videobuf2_v4l2,tidss,v4l2_mem2mem sch_fq_codel 262144 3 fuse 393216 1 ipv6 720896 30 root@tqma65xx-2gb-mba65xx:~#
- Uname -a
root@tqma65xx-2gb-mba65xx:~# uname -a Linux tqma65xx-2gb-mba65xx 5.4.109-rt55 #1 SMP PREEMPT Mon Feb 21 09:29:21 UTC 2022 aarch64 aarch64 aarch64 GNU/Linux
Here is a log captured with PuTTY that shows the complete boot from U-Boot and running the above commands:
/cfs-file/__key/communityserver-discussions-components-files/791/am65.log
If I had to guess, it would be that something with the GPU setup/configuration is wrong on my end. However, I'm sure you guys have a better idea of what it could be. Let me know your thoughts!
Thanks,
Joseph Keene