First , put the slave DSP in boot load mode, the host DSP send the code to the slave DSP through NWRITE packets. The question is I donot do anything to the slave DSP ,including the expoling the system and intilizeing the device, but the slave DSP can excute the code . I want to why , the steps in the datasheet are not all necessary?
Second, after the slave is srio boot loaded, it cannot be srio boot loaded any more. I think I must reset the slave DSP , but the slave DSP donnot have a PCI interface. In this occasion, how can I reset the DSP ? Or, there is another reason that the slave DSP cannot be srio boot load again?