Other Parts Discussed in Thread: CCSTUDIO
Hi,
I try to use RTDX communication with a DSKC6211. First of all I have tested the communication with tools in tools/RTDX menu. My system pass the internal test. after that I try to test Target to host communication. I select the .out file t2h.out in C:\CCStudio_v3.3\c6200\Tutorial\examples\rtdx\target. After long time the result is TIME OUT. RTDX communication is enable in tools/RTDX/Configuration control. Are there other setting to change?
If i try host 2 target test (with h2t.out) rapidely I receive this message
Target has not accepted the data yet!
Host-To-Target test terminated by user!
Board/CPU: C6211 Device Cycle Accurate Simulator/TMS320C6211
Hardware Mode: NONE / Pins Used: N/A
RTDX Mode: Non-Continuous
Record To: C:\CCStudio_v3.3\cc\bin\logfile.rtd
Buffer Size: 1024
Buffers: 4