This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Sizes of storage devices supported with Linux

Part Number: AM625

Our customer want to use SD card and eMMC and USB flash drive for AM625.

What is the size of each of the devices supported by Processor SDK Linux?

What is the maximum size supported by the Linux kernel for each of the devices with FAT32? Is it 32 GB?

What is the maximum size supported by the U-Boot for each of the devices with FAT32? Is it 32 GB?

What is the maximum size supported by the Linux kernel for each of the devices with ext4?

What is the maximum size supported by the U-Boot for each of the devices with ext4?

Best regards,

Daisuke