Other Parts Discussed in Thread: SYSCONFIG
Team,
Follow up question on:
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1159347/am6442-standard-ethernet-on-pru-icss-running-the-ethernet-stack-on-linux-cortex-a53/4360096#4360096
The sysconfig options are not very clear on what need to be enabled in order to support one single Standard Ethernet port on PRU-ICSS (ICSS-EMAC).
Can you please clarify the below customer question.
---------------------------
I am now trying to generate a first valid pinout for the AM64xx with this.
For the CPSW switch this looks OK.
To be able to view the pinout for the ICSS-EMAC additionally, it seems that it is not sufficient to add an ICSS-EMAC instance.
No additionally assigned pins are displayed.
Only when I add another Industrial Comms Toolkit, additional pins are assigned.
We don't want to use one of the Industrial Comms Toolkits, but standard Ethernet on PRU-ICSS. ( as described here).
Did I miss where this option can be selected, or is there no option for this yet?
Then what is the closest Comms Toolkits option that need to be enabled?
I assume that the same pins are used for standard Ethernet.
Pins for two Ethernet phys have been assigned:
We only need one Ethernet port/phy on the PRU-ICSS.
I did not find an option to remove the automatically added switch.
Does the ICSS-EMAC SWITCH config have to be used?
If the switch has to be used, can I just manually release the pins reserved for the second PHY again to assign other functions to these pins?
In this case, the internal signals for the second PHY would not be connected to the outside. Is this a problem?
Will the auto-generated SW config file will make sure that the none used ICSS-EMAC Eth pin will not conflict with the actual fonction the pin will be used for?
Thanks in advance,
A.