Other Parts Discussed in Thread: DM3730, SYSCONFIG
Hi, We are interacing an LCD on McSPI4 of DM3730. The slave (In our case LCD) needs contineous words on the MOSI line. we are able to send words one after other but there is a delay between two words and that is not acceptable by the slave. The delay is because, after transmission of one word the CS goes up and clock stops and it again start for the next word. Have tested with modified configuration (Forced bit, single mode ) as well. Kindly help on this.