Part Number: TDA4VM
Other Parts Discussed in Thread: DRA821
The DDR is configured by R5 SPL/SBL. Is there a way to check the frequency of DDR from Linux at runtime?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The DDR frequency can be determined runtime from Linux/QNX making use of the k3conf application from Linux userspace.
For J721e/TDA4VM the below command will give the DDR_PLL clock frequency:
k3conf dump clock 47
|---------------------------------------------------------------------------------------|
| Device ID | Clock ID | Clock Name | Status | Clock Frequency |
|---------------------------------------------------------------------------------------|
| 47 | 0 | DEV_DDR0_DDRSS_VBUS_CLK | CLK_STATE_READY | 1000000000 |
| 47 | 1 | DEV_DDR0_PLL_CTRL_CLK | CLK_STATE_READY | 500000000 |
| 47 | 2 | DEV_DDR0_DDRSS_DDR_PLL_CLK | CLK_STATE_READY | 1066500000 |
| 47 | 3 | DEV_DDR0_DDRSS_CFG_CLK | CLK_STATE_READY | 125000000 |
| 47 | 4 | DEV_DDR0_DDRSS_IO_CK_N | CLK_STATE_READY | 0 |
| 47 | 5 | DEV_DDR0_DDRSS_IO_CK | CLK_STATE_READY | 0 |
|---------------------------------------------------------------------------------------|
The number 47 is the Device ID for DDR as per: https://software-dl.ti.com/tisci/esd/latest/5_soc_doc/j721e/devices.html

From the output we get the DDR_PLL_CLK frequency - The clock_ID 2 in the list.
| 47 | 2 | DEV_DDR0_DDRSS_DDR_PLL_CLK | CLK_STATE_READY | 1066500000 |
The frequency above is 1066500000 Hz.
The frequency of DDR is 1066500000 * 4 = 4266 MTS(Mega Transfers per Second).
Similarly for DRA821: https://software-dl.ti.com/tisci/esd/latest/5_soc_doc/j7200/devices.html
The device_ID for DDR is 8. So the command will be:
k3conf dump clock 8
Similarly for the other TDA4 class of devices the above method can be used.
Best Regards,
Keerthy