This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM35xx: Errata Advisory 1.1.45 VIL Specification Relaxation for AC timings

Guru 10085 points

Hi.
Regarding AM35xx: Errata; Advisory 1.1.45 VIL Specification Relaxation for AC timings,
I would like to make sure about the VIL specification for AC I/O timings in the advisory.

Revision(s) Affected 1.1 and earlier
Details As a result of some timing degradations for the 3.3V and 1.8V I/Os at weak process and
high temperature, the VIL specification for AC I/O timings are changing to 0.4V.

Should I change the below value; both 0.35V and 0.8V to 0.4V in page84  of Data sheet; SPRS550C?
 



                               Excerpt from Table 3-4. DC Electrical Characteristics

Regards,
Kanae