Normal Boot Mode the dsplink application is working.we are developing DSPLink PROC External Load and Start Mode.
Please provide proper document for external load or start the DSP Running.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Normal Boot Mode the dsplink application is working.we are developing DSPLink PROC External Load and Start Mode.
Please provide proper document for external load or start the DSP Running.
Peter,
Can you give a more detailed description?
What device are you working on?
What version of Link and other tools are you using?
Are you saying that your application works OK using one boot mode, but fails in another mode?
Are you saying that you are confused by the existing Link documentation?
Dave
Hello Mr.David,
Thank you for you information.
We are using OMPL138 -(Logic PD) and the link tool version is dsplink_1_65_00_02.
I tried the following Mode of Operation is working.
: Normal Boot Mode: DSPLink loads and starts the DSP running
: DSP_BootMode_Boot_NoPwr
: DSP_BootMode_Boot_PwrDefault
But i wand to Develop the External Load and Start Mode: DSPLink does not load or start the DSP
running.
Please provide me development steps of External Load and Start Mode DSPLink does not load or start the DSP
running related information.