Part Number: AMIC110
Other Parts Discussed in Thread: SYSBIOS
Hi Sirs,
I have a project using both uart and NDK for tcp server, and I need to enable uart dma for receiving large amount of consecutive data.
I am facing same issue as the post above, when I set UART.Settings.useDma = "true"; in cfg file, can't even ping IP address,
but it will turn fine after remove UART.Settings.useDma = "true";
The post have discussion about UART and NDK/NIMU may conflict but still don't have any solution
These are the version of library I've used

Looking forward for some advice, thanks very much.