This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6746: CCS Load program

Part Number: TMS320C6746

Hello all, I have a problem with the TMS320C6746.

I am using TMS320C6746 in serial boot mode from EEPROM.

I have connected CCS for debugging to fix a bug, but the fix is not reflected.

I have checked and found that if the program is not stored in the EEPROM, it works according to the out file written from the CCS.

However, if the program is stored in the EEPROM, it runs with the program in the EEPROM even if the out file is written.

How can this phenomenon be solved?

Thank you in advance.

Suzuki