We become indebted to. I have a question about the AM572X EVM. There is an ON switch for power ON/OFF. no off switch Should I unplug the AC adapter? Also, what is the power retention time when the power is turned off? Thank you for your reply.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We become indebted to. I have a question about the AM572X EVM. There is an ON switch for power ON/OFF. no off switch Should I unplug the AC adapter? Also, what is the power retention time when the power is turned off? Thank you for your reply.
The below information is from the EVM's User Guide:
Section 2.3 Powering Off EVM
The proper procedure to power down the board is as follows:
1. Use software to gracefully power off (for example, in Linux, use the "poweroff" command).
2. If unable to use software (for example, software has crashed or does not have a shut down command), press the power button for at least 15 seconds until the power LED (D3) turns off.
3. If you need to remove the DC power jack: (a) Follow above steps to gracefully power down the board. (b) Disconnect AC power cord from the power brick. (c) Wait several seconds until the DC LED (D41) turns off (the power brick discharges its voltage). (d) Disconnect DC barrel of power brick from the board's DC jack.