Part Number: TMS320C6747
Other Parts Discussed in Thread: SYSBIOS
Hello. I am migrating a BIOS 5 in CCS 3.x program to BIOS 6 CCS 9.3.
I have problems the external processor to write in Shared memory. It can read but not writing. I have reviewed every register that affect HPI, but they have the same values than the old program. The memory map is equal than old program. Cache is disabled.
Does BIOS 6 require anything for the shared memory can be written by an external device via HPI?
thanks