This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3356: Data loss in AM3356 DCAN transmission

Part Number: AM3356

Hello:
I would like to ask about the data loss of AM3356 during DCAN transmission. The baud rate of DCAN we use is 500K, and we find that when the transmission cycle of data request is less than 1ms, it is very easy to lose data. However, we think that the mechanism of message object exists in DCAN. When data is lost, the message object is not fully used, and the transmission cycle of data request should not affect the transmission of data. Is there a problem in our understanding of data transmission? Why data will be lost when the transmission cycle is less than 1ms?
Thanks and tributes